DRV.TEMP

Description

This parameter returns the measured temperature for the specified hardware component.

Examples

Usage

The parameter can be used to track board temperatures as they change during drive operation. There is at least one control board temperature measurement (e.g., DRV.TEMP) and one power board temperature measurement (e.g., AXIS1.TEMP).

Code

--> DRV.TEMP
52.367 (Control) [degC]
--> AXIS1.TEMP
31.664 (Power1) [degC]
--> AXIS2.TEMP
32.312 (Power2) [degC]

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units degC
Range N/A
Default Value N/A
Data Type Float
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DRV.TEMP

3000h

08h

Signed32

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2021

1

2021 (0x7e5)

DRV.TEMP

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DRV.TEMP

2021

Float

Read Only

-